Other Parts Discussed in Thread: ADS8688
大家好:
系统有8个传感器通道,参数如下:
信号范围: 0 ~ 10V
信号内阻:5K
信号带宽:1KHz
ADC采样精度分辨率:1mV
其它:传感器线缆较长(4M),现场伺服和电机等设备较多,有较大的共模干扰(线缆无屏蔽层)。
ADS8688 前端电路不知是否应该用仪表运放提高抗共模干扰能力,还是可以直接利用ADS8688的高输入阻抗和差分输入能力来实现ADC精度要求。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS8688
大家好:
系统有8个传感器通道,参数如下:
信号范围: 0 ~ 10V
信号内阻:5K
信号带宽:1KHz
ADC采样精度分辨率:1mV
其它:传感器线缆较长(4M),现场伺服和电机等设备较多,有较大的共模干扰(线缆无屏蔽层)。
ADS8688 前端电路不知是否应该用仪表运放提高抗共模干扰能力,还是可以直接利用ADS8688的高输入阻抗和差分输入能力来实现ADC精度要求。
谢谢!
ADS8688这款AD的输入阻抗正好是高输入阻抗,优点就是避免再使用OP进行一个低阻抗的输出转换
如果前端需要加仪表运放有效的提高CMRR,那么后端ADC的输入阻抗要低,换句话说,需要一个低输入阻抗源的ADC。