请问:TS2DDR2811是否可以用在千兆网络变压器和RJ45之间的信号线上?
应用需求:网络变压器之后的信号接到RJ45上,这时候需要把信号从RJ45延长到另外一个连接器A。
如果连接器A有插入信号线,则打开开关。信号从连接器A到RJ45,再到网络变压器。这种情况下,RJ45口不会插入网线。
如果连接器没有插入信号,则关闭开关。信号只从RJ45到网络变压器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TS2DDR2811是可以用在千兆以太网应用上,但是TS2DDR2811的位置应该不能放在变压器和RJ45之间。
之前有客户将TS3L100放在变压器和RJ45之间是不可行的,应该是这样连接: 网口PHY-->TS3L110-->网口变压器-->RJ45连接器
因此对于TS2DDR2811应该是同样,建议还是实际验证下。