Other Parts Discussed in Thread: ADS8556, ADS1256, THS4522, ADS1271, ADS1258
你好,我在使用ADS8556时,采集差分信号时效果极差,需要对同一组两路信号都采集进AD后软件做减法实现,这个问题该如何解决?而采集一个正常的单端信号则是正常的。我使用的单端转差分电路是ADS1271中推荐使用的THS4522电路,使用ADS1256采集转换后的差分信号又是没有问题的,是不是ADS8556配置成差分输入时有问题呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
从手册上没发现8556能接受差分信号啊。手册第1页的框图,输入级SH电路的两个输入,一个是CHXX,还有一个AGND,没有办法接受差分输入。另外,既然前级已经是单端信号了,直接输入到8556不就行了,为什么还要单转双?
你评估一下ADS1258,24位125KSPS,支持差分输入。
1. ADS8556手册上已经写得很清楚了,单端输入。
2. 如果ADC可以接受全差分信号,那么输入的差分信号没必要在前端做减法,通过前端buffer/driver直接接到ADC输入即可。
3. 不建议你用软件做。通道间的失配用软件校准,效果不一定好,且有一定工作量。
4. 单端输入的AD如何采集差分信号?一个输入口也没有办法挂两个输入线啊。