This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8556如何配置成差分输入,前级的单端转差分电路如何使用?

Other Parts Discussed in Thread: ADS8556, ADS1256, THS4522, ADS1271, ADS1258

你好,我在使用ADS8556时,采集差分信号时效果极差,需要对同一组两路信号都采集进AD后软件做减法实现,这个问题该如何解决?而采集一个正常的单端信号则是正常的。我使用的单端转差分电路是ADS1271中推荐使用的THS4522电路,使用ADS1256采集转换后的差分信号又是没有问题的,是不是ADS8556配置成差分输入时有问题呢?

  • 从手册上没发现8556能接受差分信号啊。手册第1页的框图,输入级SH电路的两个输入,一个是CHXX,还有一个AGND,没有办法接受差分输入。另外,既然前级已经是单端信号了,直接输入到8556不就行了,为什么还要单转双?

  • 你好,当时想法是使用差分输入,消除共模干扰的,本来想选用ads1271的,1271是全差分输入运放,后来由于种种原因选择了ads8556,。所以说8556就是不带差分输入功能对吧?它内部对每一个通道都是有一个采保器的,而全差分输入ad是一对差分信号做过减法后在进入采保器的对吧?那我能用软件上的方法解决这个问题吗?或者你有过使用单端输入的AD采集差分信号的范例吗?

  • 你评估一下ADS1258,24位125KSPS,支持差分输入。

    1. ADS8556手册上已经写得很清楚了,单端输入。

    2. 如果ADC可以接受全差分信号,那么输入的差分信号没必要在前端做减法,通过前端buffer/driver直接接到ADC输入即可。

    3. 不建议你用软件做。通道间的失配用软件校准,效果不一定好,且有一定工作量。

    4. 单端输入的AD如何采集差分信号?一个输入口也没有办法挂两个输入线啊。

  • 好的,我要使用是的是同步采集AD,所以还是会是用8556,我重新设计AD前端电路就好了,谢谢你的答案了