最近在做一个项目 需要选一款具有双极性电压输出的DAC芯片,输出电压范围为-4V~+4V,用来产生占空比可调的锯齿波,后续电路不用增加运放,想请教一下有没有这种芯片。另外有人说DAC的输出阻抗较大,想得到较为理想的输出波形,后续电路仍需要增加运放,想请教一下是否真是这样。谢谢大家!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
都有各自的优点和缺点吧,单极性的话,可能在噪音上的处理要弱一些,但是成本相对要低一些。尤其在高传输速率和长传输距离的应用当中,一般建议双极性,即使两端都有噪音耦合进入,但由于是差分信号,相互抵消,抑制噪声能力更强,但成本要比单极性要高。
运放选择以下就可以了
OPA277
OPA704
OPA727
手册的19页图47有介绍
hi,我按照DAC8831的datasheet使用双极性的模式,电压基准芯片选择REF3330,DAC输出+-3伏。
现在一切工作正常。想问:如果想把+-3伏再经二级放大的话一定要用隔离运放吗?为什么?可以推荐一下型号吗?希望输出+-10伏,负载80-150千欧。
谢谢。