This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112 设置上下限温度报警的问题。中断模式

比如现在温度40 ,我设置上限41,下限39, 如果温度先超高41,有中断,然后低于39有中断。   另一种情况比如现在温度40 ,我设置上限41,下限39, 如果温度由现在的40直接低于 39,不会产生中断 。 请问,这个ic只能先比较高,让后才能比较低吗?
  • 大家帮帮忙,谢谢啦
  • Kaeer, 您好:

    请参考数据手册 7.5.4的interrupt mode(TM=1)以及Figure16,当温度超过上限或者低于下限时,都会导致Alert 引脚信号的变化,并不需要先高于41再低于39。这种模式是满足您要求的。但此时只能通过Alert引脚知道超出了温度范围,但并不知道是高于还是低于门限温度。

    另外请参考7.5.3.4,为了防止噪声对温度比较结果的影响,您可以设置触发Alert前连续故障的次数。

    希望我的回答解决了您的疑惑。

    谢谢,祝您新年快乐!

    Marc