This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1115读取12V电压问题

Other Parts Discussed in Thread: ADS1115

需要读取最大到15V电压,精度1mV以内。通常情况是读取12.000V电压。用的0.1%电阻,经过10K和2K电阻分压后至ADS1115读取,ADS1115供电电压4.7V左右,增益为1,连续读取取平均值。但是想请教如何减少由电阻分压带来的误差。除了使用程序去修正外。因为需要量产。