使用TXB0104做串口电平转换,VCCA 1.8V VCCB 3.3V OE 1.8V 。B端接3.3V cpu的TX\RX,A端接1.8V器件的g_RX\g_TX。器件向CPU发送数据,CPU接收正常,即g_TX-》RX正常,但是CPU向器件发送数据异常(即TX-》g_RX)。测量电压,TX端只有1.3V左右,g_RX为0.原设计电路是没有任何上拉、下拉一类的,都是直连。后来飞线添加了一些上拉、下拉、电容等测试,没有任何改善。看手册好像没什么特殊控制的地方,因此搞不懂了,特此求助。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TXB0104做串口电平转换,VCCA 1.8V VCCB 3.3V OE 1.8V 。B端接3.3V cpu的TX\RX,A端接1.8V器件的g_RX\g_TX。器件向CPU发送数据,CPU接收正常,即g_TX-》RX正常,但是CPU向器件发送数据异常(即TX-》g_RX)。测量电压,TX端只有1.3V左右,g_RX为0.原设计电路是没有任何上拉、下拉一类的,都是直连。后来飞线添加了一些上拉、下拉、电容等测试,没有任何改善。看手册好像没什么特殊控制的地方,因此搞不懂了,特此求助。