This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运放和AD的选择

Other Parts Discussed in Thread: ADS8519

需要采集压电式加速度传感器产生的低频信号,1kHz以下,采用电荷放大器将电荷信号转成电压信号(几十mV),然后经过低通抗混叠,积分,和高通,再经过放大给AD采集,AD拟采用ADS8519的±10V范围,AD采集频率10kHz。

问题1:低通抗混叠的频率选多少为好?

问题2:有什么合适的四运放可以用?

问题3:低通抗混叠放在积分前好还是放在AD前比较好?

  • 关于 4运放, 对于信号频率低, 精度高, 可以采用低失调地偏置的精密运放. 具体选型还得看你对信号的精度要求

    关于滤波, 个人感觉你还可以放在 ADC 后的软件里面. 运放前端用个简单的低通就行了