使用DA3482时,外部已经有1G的时钟,但还需要产生频率为1G/16的OSTR信号作为同步信号,除了分频器CP1803这种,还有什么其他类型的更简单易用的芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用DA3482时,外部已经有1G的时钟,但还需要产生频率为1G/16的OSTR信号作为同步信号,除了分频器CP1803这种,还有什么其他类型的更简单易用的芯片?
你好,
分频的一般都是通过计数器来实现的,请问你的系统还有哪些器件,1G 的时钟由什么芯片合成的?
你好,
可以考虑时钟分频器或者合成器,具体选型可在以下网址:
http://www.ti.com/clock-and-timing/overview.html
可以考虑LMK01000这类时钟器件,能够支持的最大频率为1.6Ghz,分频系数可以从2~510.但是要看下输入输出电平是否符合要求。