Other Parts Discussed in Thread: DAC3162, AFE7225
工作速度最大300MHz,带宽大于30MHz,量化12bit,输出频率15MHz左右,带外抑制大于50dBc,采样速率大于300MHz,输出功率-2dBm至2dBm。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输出功率最大2dbm?才1.6mW哦,是不是写错了哦
除了输出功率这个限制,如果量化只能是12bit的话,推荐DAC3162,当然resolution选择更高的话,就有更多的选择。
具体的选型请参看:www.ti.com.cn/.../high-speed-dac-greater-10msps-products.page
可以根据你的需要进行选择。
谢谢!因为这个DAC还想要外加一个放大器,输出±2dBm是要求的,输出的工作频率15MHz±5MHz,是要求的。