我在网上买的加上稳压电源和放大器的DAC,核心是DAC8563,我利用SPI通信,最后我测试的时候AVDD=5.5V,DIN,SCLK,SYNC均为3.3V的控制信号,LDAC和CLR均接地,然后没有输出。我的控制器是TMS320F28027。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在网上买的加上稳压电源和放大器的DAC,核心是DAC8563,我利用SPI通信,最后我测试的时候AVDD=5.5V,DIN,SCLK,SYNC均为3.3V的控制信号,LDAC和CLR均接地,然后没有输出。我的控制器是TMS320F28027。
你好,
DAC用5.5V供电时,高电平最低为0.7*AVDD=3.85V,而你的SPI信号高电平为3.3V,所以没有输出。建议DAC8563用3.3V供电,或者使用电平转换芯片,然后再进行测试。
你好!
你应该使用的是内部Reference,内部Reference是2.5V,所以VOUTA和VOUTB最多输出2.5V。如果想要输出更高的电压,可以使用外部Reference,比如REF5050,但是切记Vrefin最好不要超过AVDD。