手册上说OE管脚的输入参考VCCA,现在我的VCCA为2.8V,OE管脚输入的高电平为3.3V,请问会有什么问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册上说OE管脚的输入参考VCCA,现在我的VCCA为2.8V,OE管脚输入的高电平为3.3V,请问会有什么问题吗?
你的VCCB是多少?如果是5V的话,OE可以到5V
手册第五页6.3章节有描述
OE input 1.2 V to 3.6 V 1.65 V to 5.5 V VCCA × 0.65 5.5
您好,我的VCCB电压为3.3V,VCCA电压为2.8V,OE高电平是3.3V,不知道这样可不可以。
之前我的OE电压是2.8V的时候工作没问题。。
OE参考的是VCCA,最高为VCCA的电压,如果您现在接到3.3V的话,参考VCCB是不正常的。
Pengyu An1 说:您好,我的VCCB电压为3.3V,VCCA电压为2.8V,OE高电平是3.3V,不知道这样可不可以。
之前我的OE电压是2.8V的时候工作没问题。。