This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请帮忙推荐一款ADC和运放?急!急!急!

Other Parts Discussed in Thread: ADS8681, ADS8329, THS4031

请TI专家帮忙推荐一款ADC:

1、16bit及以上,速率1M及以上,SPI通讯,单通道,输入范围5V,推荐一款性价比比较好的;

2、配合以上ADC再推荐一款运放,高精度,低温票的。

主要用途是用来采集单通12V的电池串联组,现在没有能够采集12V单通电池的专用IC,所以想

通过差分将电压缩减下来,用ADC来采集,整个通道精度希望做到0.2%及以下,有好的方案也可以推荐。          

                                                                                                    非常感谢!

需要详细询问需求,可以电话或者邮箱联系:15884484844     huangmin@scaeme.cn