请TI专家帮忙推荐一款ADC:
1、16bit及以上,速率1M及以上,SPI通讯,单通道,输入范围5V,推荐一款性价比比较好的;
2、配合以上ADC再推荐一款运放,高精度,低温票的。
主要用途是用来采集单通12V的电池串联组,现在没有能够采集12V单通电池的专用IC,所以想
通过差分将电压缩减下来,用ADC来采集,整个通道精度希望做到0.2%及以下,有好的方案也可以推荐。
非常感谢!
需要详细询问需求,可以电话或者邮箱联系:15884484844 huangmin@scaeme.cn
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请TI专家帮忙推荐一款ADC:
1、16bit及以上,速率1M及以上,SPI通讯,单通道,输入范围5V,推荐一款性价比比较好的;
2、配合以上ADC再推荐一款运放,高精度,低温票的。
主要用途是用来采集单通12V的电池串联组,现在没有能够采集12V单通电池的专用IC,所以想
通过差分将电压缩减下来,用ADC来采集,整个通道精度希望做到0.2%及以下,有好的方案也可以推荐。
非常感谢!
需要详细询问需求,可以电话或者邮箱联系:15884484844 huangmin@scaeme.cn
ADC可以参考ADS8329:2.7V~5.5V, 16 Bit 1MSPS Serial ADC
datasheet中和ADS8329一起使用的是THS4031。 这款运放供电电压最大30V,所以采集12V也是没问题的。
或者如果您想给ADC差分输入的话,可考虑选择全差分运放。