LL连接IN2P,LA连接IN2N,LA连接IN3P,RA连接IN3N。一般情况下采样出来的数据都是在24位AD采样的中间位置而且数据也是正常的(实验室模拟仪出来的信号接上去都没有问题),但有出现数据漂移的情况:就是IN2或者IN3采样出来的数据刚开始就大于中间值,然后慢慢往0x7FFFFF(正值最大)漂移,最后出现0x7FFFFF(正值最大),从而导致采样的波形被0x7FFFFF淹没掉了,没有数据了。而且IN3出现的几率很大,还望能得到解决。在线等
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用的电压是AVDD=+2.5V,AVSS=-2.5V,AVDD=+3.3V。参考电压使用芯片内部的+2.4V,ADS1298内部的PGA放大倍数为6倍的情况下测试的。极化电压一般为0~300mV,放大6倍后最大也只是1.8V,不会超过2.4V。采样出现0x7FFFFF说明进AD采样的电压已经超过或者正好是2.4V。
你好,12lead的正常接法应该是lead1=LA-RA,Lead2=RA-LL, Lead3=LL-LA。 由于lead的阻抗会缓慢变话,所以低频基线漂移的确存在,频率一般在0.05Hz,采用AC耦合或者添加滤波器来滤除。这种漂移至max的现象最有可能就是lead接触不良,你在采用模拟器信号实验一切正常更能说明这一点。如何检测lead off,请参考这篇文档。www.ti.com/.../sbaa196.pdf
1、我用了直流的导联脱落检测(参照数据手册的设置),正常情况下一根一根拔下来都能正常检测。但出现上面的的漂移情况下也没有报导联脱落。
2、LL连接IN2P,LA连接IN2N,LA连接IN3P,RA连接IN3N,再把IN2P、IN3P、IN3N作为右腿驱动。1)检测导联脱落的时候设置IN2P、IN3P上拉,IN3N下拉,正常一根脱落都没有问题,但是要是LL(IN2P)、LA(IN3P)一起脱落,其他的没脱落的情况下就会报LL、LA、RA、RL(右腿驱动)一起脱落,这个问题不知道如何解决?2)检测导联脱落的时候设置IN3N(AR)、IN2P(LL)上拉,IN3P(AL)、IN2N(AL)下拉,检测导联脱落时:LL脱落正常检测,AL脱落时会出现LOFF2N和LOFF3N都为1,AR脱落时时LOFF3P为1(3通道IN3的P端是AL,N端为AR,看数据手册情况应该是AL脱落时LOFF3P为1,AR脱落时LOFF3N为1,这个和实际结果相反,还是我的理解有问题,难道是通道P端下拉、N端上拉会导致读出来的导联脱落也是反的,3通道上拉的标志在LOFF3P中,3通道下拉的标志在LOFF3N中------>我看数据手册的理解是3通道P端的导联脱落在LOFF3P、3通道N端的导联脱落在LOFF3N,不管设置直流检测导联脱落时是上拉或者下拉)。
1 如果不是导联脱落的问题,这样drift到0x7FFFFF就很有可能是RLD的问题。请确认RLD运放是否开启,RLD运放的正端参考源配置。
2 1)用RA,LL,LA来做RLD的前提是都在非导联脱落的状态下。在你的导联脱落时,通道被上拉至AVDD,这样的你RLD REF会变高,比较器的REF也会变,这样就会导致导联工作不正常。2)你的理解是正确的,不论上下拉,P的导联脱落状态都存在LOFFxP里。我来测一下再回答你这个问题。
你好,我用EVM做了相关导联脱落测试,的确是上下拉变换之后,导联脱落的标志也会相应变化。我已将此问题反馈给美国团队。谢谢。