Other Parts Discussed in Thread: TXS0108E, SN74AVC8T245
你好,现在用TXS0108E进行电平转换时(A通道是2.8V电平,B通道是3.3V电平),当数据速率是50MHz进行转换时输出信号没问题,当把数据速率提高到80MHz以上时信号输出电平不正常,请问是该芯片不能支持这么高速率数据转换吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TXS0108E, SN74AVC8T245
你好,现在用TXS0108E进行电平转换时(A通道是2.8V电平,B通道是3.3V电平),当数据速率是50MHz进行转换时输出信号没问题,当把数据速率提高到80MHz以上时信号输出电平不正常,请问是该芯片不能支持这么高速率数据转换吗?
SN74AVC8T245
Maximum Data Rates
– 170 Mbps (VCCA < 1.8 V or VCCB < 1.8 V)
– 320 Mbps (VCCA ≥ 1.8 V and VCCB ≥ 1.8 V)
另外想确认一下SN74AVC8T245是否同时支持推挽输出和开漏输出两种数据转换?