Other Parts Discussed in Thread: ADS8634, ADC124S101, ADS1234
请FAE推荐几款TI的AD片子:4通道,每通道采样频率1M,精度12-16皆可,有价格更好。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS8634, ADC124S101, ADS1234
请FAE推荐几款TI的AD片子:4通道,每通道采样频率1M,精度12-16皆可,有价格更好。
Hi kang yu,
请问一下几个问题,以便确认ADC的选型,谢谢。
1.输入信号的类型:单端信号,差分信号,单极性,双极性?
2.数字接口类型:串口、并口SPI, I2C等等
3.需要集成PGA吗?
4.是否需要外部参考?
5.是否需要同步采样?
6.能提供什么样的电源供电?
7.功耗,体积有限制吗?
ADS8634,4通道输入,最高采样频率1M。这是ADC转换核的采样频率,平均到每通道,采样频率就只有250K了。不知道我的理解对不对?
考虑满足条件的片子有限,先不考虑输入信号的类型、数字接口类型、外部参考。需要集成FPGA,不需要同步采样,功耗、体积无限制。
考虑满足条件的片子有限,先不考虑输入信号的类型、数字接口类型、供电方式。集成FPGA,不需要需要同步采样。注意每通道采样率需达到1M。
ADS8634只有一个ADC, 前端集成的是一个4路输入的多路选择器MUX. 对于这个ADC而言,它的采样率最高达到1Msps。
麻烦Kailyn Chen重新推荐AD片子,ADS8634不满足我的采样要求,采样频率不够。4通道同时输入,每通道采样速率1M。若4路输入,AD内部有多路选择器,则ADC转换速率要达到4M。或2个ADC,每个ADC转换速率要达到2M。或内部有4个ADC,转化速率1M即可。