This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

新开一贴,询问关于ADS1299实际应用的问题

Other Parts Discussed in Thread: ADS1299, ADS1298

使用ADS1299有一年多了,看着TI论坛里面的询问越来越多,抛开一些初始化和SPI相关的问题不说,大家问的最多的就是1.bias ,2.单双端输入,3.噪声干扰,

实际使用中我也遇到了很多问题,有很多也没办法解决。然后看论坛上面的很多TI工程师也没给出一个比较准确的回答。所以想综合一下问一下(本来想去寻求一下TI的FAE支持一下这个芯片的,中国好像只有办事处,顺便还调戏了一下欧洲的客服小妹,最终也没有结果)。

1.bias:bias和心电里面的右腿电路很像,第一次看数据手册,看到一堆的带bias解释的引脚,一头雾水,后面才渐渐区分各自功能,目前我理解的bias就是各输入通道的信号和(大概理解为共模信号?)然后反向输出给人体,从而抑制共模信号,有错误请指出,都是在学习中。那么如果配置成8通道全部链接到bias,假设有1-2通道没有连接到人体,是否这两个通道的无效信号会对bias产生影响,从而给其他通道带入干扰,假设是的,不适用的通道是不是要从bias断开(我理解软件设计会要求动态刷新bias和各通道的连接状态?),其次,bias接到人体上某一点,离bias点越远的点是不是抑制的效果越差(人体阻抗的原因),那么bias反馈的倍数要怎么调节。

2.单双端输入,单双端输入其实很好理解,我相信大部分人都是用的单端输入,有需要双端的话通过软件去处理会更简单方便,那么经过我的初步测试,发现双端输入比单端输入的噪声要小,特别是那些做多片级联的,然后呢是N极输入的噪声比P极输入的噪声要小。

3.噪声干扰:这里的噪声干扰不是指芯片的的低噪,电源带入的噪声等等,而是指实际应用上人体输入的噪声,ADS1299,TI给的定义是集成模拟前端,我的理解是这个芯片的位置应该处在信号从电极进来的第一级,前面最多是一些阻容的无源器件,但是现在按照评估板来做,发现实际使用有很大的问题(接信号发生器没有问题),然后输入阻抗测了貌似小于10M(手册上写1000M,500M),那么请问ads1299的输入通道的前面到底需不需要加芯片,加什么芯片,仪表运放,还是普通运放,还是那些什么特殊功能的运放,然后输入阻抗的匹配要怎么做。

大致是以上的综合问题,还有一点要问一下各位坛友哥哥们,有没有用ads1299做出成熟能用的来啊,help啊