将Input Multiplexer Control Register (Address 01h)值设为0x88,均连接到AINCOM。为什么末六位还不稳定?!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问你的采样率采用的是多少,你的PGA采用的是多大?这两项会影响其分辨率,方便给出你的电路图吗?另外,推荐看一下datasheet上的page13和page14的内容。
Hi:
在您的电路中采用的高精度基准源REF195, 如果是这样的话,输入电压需要大于5.2V以上,否则输出电压5V输出会因为Vdrop偏离而造成严重的精度损失。输出电容也不需要100uF这么大,选用1~2.2uF陶瓷电容即可.ADC的AVDD.DVDD电容也推荐4.7~10uF陶瓷电容。
两外就是要注意数模隔离,各信号GND端点接GND Plane.