This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DAC3162输出是电流型的,这个能不能转换成电压型的,复杂吗?或者帮我重新选型一下,参数:工作速率300MHz,采样带宽大于30MHz,量化12bit,输出的频率15MHz+-5MHz,内部有放大器,输出功率0+-2dBm,即0.83mW至1.6mW,带外抑制大于50dBc,谢谢!!!
1. 这类高速DAC都是电流输出的,需要在输出端接电阻实现电流转电压。你所谓的“内部有放大器”,实际上,3162内部应该是有的,能够驱动外部的电阻,实现电流转电压的功能。
2. 至于输出功率的问题,2dBm的信号,峰峰值是0.8V,你可以用输出端接电阻的方法来实现。这种方法详见手册19页的例子。你的DAC后级接什么电路?如果后级接一个全差分的电路,信号链可以是DAC->电阻->滤波器->后级差分电路;如果后级是单端电路,则信号链可以是DAC->电阻->滤波器->双转单->后级单端电路。双转单用一个速度稍高点的运放应该可以实现,但是还是需要你明确一下噪声和THD方面的需求。
3. 带外抑制需要你自己搭电路实现,大约3到5阶的低通或者带通应该够了。