This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS122C04的咨询

Other Parts Discussed in Thread: ADS122C04, ADS1220

ADS122C04 寄存器配置可以正确读写,但是读取数据的时候,读出的数据全都是0,代码如下:

寄存器配置值为:static uint8_t C_ADS1220_Par_Default_W[4] = {0x91,0x08,0x00,0x00};

uint32_t ADS122C_GetData(void)
{
uint8_t ret;
uint32_t L_ADS122C_Data = 0;
uint32_t L_ADS122C_Buf[N];

ADS122C_DRDY();

ret = ADS122C_Config_Init();

if(ret == 1)
{

ADS122C_StartConversion();

for(uint8_t i = 0; i < N; i++)
{

while(ADS122CDRDY_IN);

delay_ms(10);

ADS122C_Read_Data(&L_ADS122C_Buf[i]);

}

for(uint8_t i = 0; i < N; i++)
{

L_ADS122C_Data += L_ADS122C_Buf[i];

}

L_ADS122C_Data = (uint32_t)(L_ADS122C_Data / N);//取平均值

}
else
{
//异常
L_ADS122C_Data = 0;
}

ADS122C_PowerDown();

return L_ADS122C_Data;
}

请问是为什么呢?