请问,如果不用差分输入,ADS1114-Q1可以检测两路模拟信号吗?如果可以的话,芯片的3脚(GND)就是两路信号的地吧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问,如果不用差分输入,ADS1114-Q1可以检测两路模拟信号吗?如果可以的话,芯片的3脚(GND)就是两路信号的地吧?
不可以检测两路。只是一路差分输入,单端输入的话,另一路接地。
如果需要两路,可以采用ADS1115,但ADS1114 和ADS1115内部均集成了一个ADC,两路输入的话也是需要通过前端MUX来配置选择哪一路输入到ADC。 不能同时检测。