TI专家:
你好!
关于ADS8694/8698中阈值设置及报警规则问题有些疑问,望解答。
在数据手册8.3.11中有一些说明,ADC输出数据与阈值会通过内部比较器做比较来确定ALARM信号是否被触发,其中ADC输出数据是18位,范围是0-262143,而阈值为16位数据,范围是0-65535,这两个数据长度不对等,请问这是如何比较的?
在此章中指出ALARM会在第16个时钟周期的下降沿会改变状态,请问这个时钟周期从哪里开始算起?是从CS信号的下降沿还是从SDO开始输出数据算起?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI专家:
你好!
关于ADS8694/8698中阈值设置及报警规则问题有些疑问,望解答。
在数据手册8.3.11中有一些说明,ADC输出数据与阈值会通过内部比较器做比较来确定ALARM信号是否被触发,其中ADC输出数据是18位,范围是0-262143,而阈值为16位数据,范围是0-65535,这两个数据长度不对等,请问这是如何比较的?
在此章中指出ALARM会在第16个时钟周期的下降沿会改变状态,请问这个时钟周期从哪里开始算起?是从CS信号的下降沿还是从SDO开始输出数据算起?
这个在数据手册中说的不是很详细,请问您有没有相关的技术资料或者是做过一些验证?
没有实际用过这个芯片,自己实际软件配置下,运行两次就搞明白到底是如何设置的了,比研究数据手册也快。
你好,
ALARM信号是在CS拉低后的将寄存器的16为数据与ADC输出的前16个MSB进行比较。