Other Parts Discussed in Thread: THS8200
最近在配置dm6467+ths8200的VGA输出,ths8200输入20bit ,4:2:2 ,Ycbcr,准备输出XVGA 1280X1024,108Mz。按照ti给出的配置文件,配置ths8200的寄存器。但是没有显示,显示器提示“超出显示范围”,用示波器测试发现HS_OUT只有49Khz,VS_OUT只有50Hz。正常值HS_OUT应该为64.10KHZ,VS_OUT应该为60.24HZ。个人检查了好几遍寄存器,没有发现任何问题。请问,会是什么原因呢?
对ths8200的配置有如下疑问:
1,我的HS_IN与VS_IN没有使用,3.3V上拉。FIDIN也没有使用,接地下拉。请问这样处理是否正确?
2,ths8200的时钟用的是VPIF的输入时钟,峰峰值为2.6V,而不是一般有源晶振的5-6V,请问这对ths8200有影响么。
望不吝赐教,谢谢!