Other Parts Discussed in Thread: AFE5801
请问AFE5801在写寄存器的时候,可以使CS信号拉低48个周期,连续写两个寄存器吗?很急,求解释。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AFE5801
请问AFE5801在写寄存器的时候,可以使CS信号拉低48个周期,连续写两个寄存器吗?很急,求解释。
谢谢你的回答,还有一个问题。手册上第18页上有关复位的问题。为了节省功耗,采用硬件上电复位的方法,即在RESET脚通过一个10K欧姆的电阻连到1.8VD,那么在开电源的时候就完成了复位的操作。现在问题是上电了之后,RESET脚连了1.8VD,一直保持这样吗?RESET脚是否要重新拉低?是通过写寄存器的方法拉低吗?
谢谢您的帮忙。我正在测试AFE5801这个芯片。我用静态方式写一条增益曲线,用来放大输入的500mV正弦波信号。寄存器只是设置了TGC_REGISTER_WREN为1,其他寄存器设置为默认值。然后拉低CS信号,每48个时钟周期写一个增益值(粗调+细调)。复位信号我没有设置,用了一个上拉电容接上1.8VD,然后再接了一个10K的下拉电阻接地,利用电容的充放电完成复位。我用示波器测量SPI的信号,都是正确的。但是我在数据输出端测量,一直没有信号输出,到底是什么原因?难道是复位信号的设置出错了?
您好,图中VCM是没有跟地相连的,而且单端输入,所有INxM已经和地之间通过100nF的排阻相连了。问题出在哪儿了?