你好,
LMX2594EVM Reference Pro 不与电脑连接,请问如何解决?
多谢!
王斌林
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
LMX2594EVM Reference Pro 不与电脑连接,请问如何解决?
多谢!
王斌林
您好,请参考user guide检查硬件的设置是否OK
你好,
按照user guide操作,测试环境及方法为:
1,使用仪表:笔记本电脑,Agilent E4405B 频谱分析仪,40dB衰减器,直流电源。
2,直流电源输出设置为3.3V,限流 450mA。
3,使用方法:按照 LMX2594 EVM Instructions – 15-GHz Wideband
Low Noise PLL With Integrated VCO User's Guide 连接电源,频谱仪,笔记本,EVM板。按照 User's Guide给不用的端口接50欧姆负载。
4,测试步骤:连接好后,打开测试工具TICS Pro,打开电源 3.3V,待机时电流约为170mA,工作后电流约为390mA。频率、功率都可以调节。测试时频率设置为7GHz。
5,故障现象:正在工作时,突然没有输出,测试工具显示USB无连接。
TI你好,
因当前任务紧,没有太多时间等待最终解决方案。这个问题能否这样处理,
1,先给我们换一块Reference Pro 板,让我们继续测试LMX2594EVM。把坏的Reference Pro 板寄给TI继续分析,寻找问题点。
2,为解决此问题,我们在TI官网上研读了大量与Reference Pro、LMX2594EVM、TICS Pro、USB2ANY等相关文献。经我司分析,初步判断,Reference Pro板上的U1输出电压太低,约为0.7V(在Reference Pro板上的C3、C20上测试),导致U4(M430)不能正常工作,不能与电脑连接的故障。我司打算尽快自行修复Reference Pro板,只去掉U1,看看结果如何。