This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教dac复位电路问题

Other Parts Discussed in Thread: DAC121C085, DAC121S101

Ti专家,你好

    想请教一个关于Dac复位电路问题,

    1、在使用Dac121c085的时候,如果频繁开关机,会出现输出锁定的情况,经手册描述和咨询,是因为这个芯片的复位电路需要电压小于200mv后才能可靠复位,否则可能出现输出锁定。请问这个是否有解决方案可以避免这个问题。

   2、如果1无法避免这个问题,请问有其他类似芯片,但是不存在这个问题的DAc推荐吗,12bit -14bit。

      我看了一下DAC121S101/-Q1手册,在复位部分并没有提及需要小于多少电压才能可靠复位的问题,请问是不是这个芯片就不存在Dac121c085的复位问题。是不是只要电压低于多少就复位。高于多少就能工作。

     谢谢。

  • 频繁开关机是想验证什么功能吗?因为芯片内部集成复位电路是我们想要的结果,有些芯片没有POR电路,有时候我们还需要外加,来保证正常复位,芯片正常工作。
    那我想,需要频繁开关机的话,即使不含有POR 电路,我的建议也是正常的开机关机时序,这样才能保证芯片的性能。
  • 谢谢您的答复

    可能是我没表述清楚,是在某些情况下可能出现类似频繁开关机现象,我们在应用dac的时候发现dac如果在没有完全到达符合复位电平前提下(DAC121C085是小于200mv)复位(vcc上有电容,电压下降到0需要一定时间),dac就可能出现输出锁死,但是通讯正常的情况,这个是我们不想看到,所以请教专家如何避免这个问题,或者是否有新的芯片,复位电路原理和这个不一样,不会出现这个问题。

    还是说一般dac都存在这个问题,需要额外的外部来处理才能解决这个问题。

  • 请问能否提供下原理图以帮忙判断,有可能是电源去耦电容配置的问题
  • 请参考以下来自产品线的回复:

    It could be tackled by using a 0.1uF and a 10uF capacitor on the power supply pin of the DAC. Please make sure the 0.1uF capacitor is placed close to the device pin. In case the power supply is shared with other noisy devices and circuits on the system, it may be a good idea to put a ferrite bead in series with the power supply before the 0.1uF capacitor. So the sequence should be as follows:

    Power Source --> 10uF --> Ferrite bead --> 0.1uF --> DAC Power Pin

    This should solve the problem if the power supply noise is getting coupled conductively. In case it is getting coupled by other means such as electrostatic or electromagnetic, then they should look at the layout and make sure the DAC has other means of isolating this noise, e.g. emi shields etc.

    Hope that answers your question.

    链接:
    e2e.ti.com/.../2571442
  • 非常感谢您的回复,我们根据您的建议来修改我们的设计。

    下面是我们目前的电路图,麻烦请您指正。谢谢。

  • 这个是我们目前在dac电源端监测到的关机时候电压波形图,如过在关机后1.2S左右就是在图中标出的200mv左右的点再次上电的话,DAC就会出现我前面描述的问题,输出锁定,但是通信正常。

    我们想求助的问题是,如何避免这个问题。

  • 应该是ADR435这颗器件的问题,是一个电压参考,换一个高精度的LDO试一下吧

  • 感谢您的专业指导。

    万分感谢。

  • 如果对您有帮助的话,还请帮忙确认下答案,帮助结贴,谢谢