This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于使用AFE做血氧传感方案的问题

Other Parts Discussed in Thread: AFE4410, AFE4490

我们实验室的一个项目,需要测量皮肤浅表层毛细血管的血氧饱和度。因为是皮肤浅表层,而且致力于全身任何地方都能测量,传统的光电容积脉搏波信号测量的方法不能用,AFE的LED驱动电路和ad转换等功能还是可以使用的。打算增加光源的个数来消除未知数,初期通过理论推导,基本确定需要使用三到四个光源,但是能够支持四个光源的模拟前端(AFE4410等)都是政策保密的,没有用户手册。

我在想是否可以把两个支持双光源的模拟前端串在一起使用,就可以达到四个光源的效果。但是,我不确定AFE4490等模拟前端的工作方式,是单片机控制光源还是模拟前端自己控制光源,如果我使用两个模拟前端串在一起再配上单片机是不是可以控制四个光源交替发光;还是每个AFE都是独立工作的,无法组合在一起使用。想请教一下。

当然如果有更好的方案也请各位指导:Xinming@vip.henu.edu.cn