您好,TI技术支持。有个项目需要采集250mV的外部电压信号,并且需要将外部电压与内部控制电压进行隔离,有意选择贵公司的AMC1304M25这款芯片。但是使用方面有些疑问,该芯片的通信接口是SCLK和DOUT两根信号线,通过datasheet不是太了解其使用方法。如果将这两根线连接至MCU的SPI_CLK和SPI_DOUT引脚上,是否可以获取ADC转换值?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TI技术支持。有个项目需要采集250mV的外部电压信号,并且需要将外部电压与内部控制电压进行隔离,有意选择贵公司的AMC1304M25这款芯片。但是使用方面有些疑问,该芯片的通信接口是SCLK和DOUT两根信号线,通过datasheet不是太了解其使用方法。如果将这两根线连接至MCU的SPI_CLK和SPI_DOUT引脚上,是否可以获取ADC转换值?
您好,谢谢解答。能否帮忙讲解一下AMC1304的SCLK与DOUT之间的时序关系?AD转换结果值通过DOUT端口的占空比信号输出,该占空比信号的周期如何确定?发送多少个CLK信号才能使其完整输出?