This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下ADS1243和ADS1256选型问题

Other Parts Discussed in Thread: ADS1243, ADS1256

1. 我们需要处理几十uV左右的小信号,要求分辨率在10uV左右,请问ADS1243和ADS1256那颗更好?

2. ADS1243和ADS1256除了寄存器地址不同外,在使用方法上是否一致(例如,先设通道,PGA,再等ready信号,再读值)?

感谢,盼复!!!

    • ADS1256
    • 24 Bits, No Missing Codes
      • All Data Rates and PGA Settings
    • Up to 23 Bits Noise-Free Resolution
    • ±0.0010% Nonlinearity (max)
    • Data Output Rates to 30kSPS
    • Fast Channel Cycling
      • 18.6 Bits Noise-Free (21.3 Effective Bits) at 1.45kHz
    • One-Shot Conversions with Single-Cycle Settling
    • Flexible Input Multiplexer with Sensor Detect
      • Four Differential Inputs (ADS1256 only)
      • Eight Single-Ended Inputs (ADS1256 only)
    • Chopper-Stabilized Input Buffer
    • Low-Noise PGA: 27nV Input-Referred Noise
    • Self and System Calibration for All PGA Settings
    • 这个介绍, 性能优于 ads1243

  • 感谢您的回复。

    ADS1243的PGA最大倍数为128, ADS1256PGA的最大倍数为64,请问这个指标需要靠考虑吗?

    另外,在ADS1256上验证一个50uV左右的信号时,发现PGA设为1和PGA设为64时,采样出来的电压值是一样的,没有成倍数增长。这个是如何解释?

    谢谢!