This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1217等,分DVDD和VADD两个电源的,是怎么使用呢



是需要2个电源隔离供电吗,还是接在一起,对测量精度有多大影响

比如: 电路单片机供电VDD=5V,有一路DCDC隔离出AVDD=5V,我在AD供电的时候是不是DVDD就接单片机的电源,AVDD接DCDC隔离的5V,而单片机IO和ADSPI引脚就不需要光耦隔离了?

  • 你好,电源隔离的本质在于隔绝数字部分的噪声通过电源耦合进模拟电路影响其噪声指标。如果要追求低噪声表现不推荐用DCDC给AD模拟部分供电,尽量使用用low noise的LDO给模拟部分AVDD供电。数字部分DVDD就用VDD供。IO属于数字已属于数字电路部分,不需要再进行隔离了。另外PCB布局时要注意地的隔开,请参考http://www.ti.com/lit/an/sbaa052/sbaa052.pdf