你好,我们在评估一个关于手术室监护的项目,考虑采用ADS1298/1299的方案,我们目前已搭建起基于1298的采集系统,如果要增加抗电刀干扰的能力,请问难度大不大,还有多少工作要做。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于这个问题,应该从两方面的标注文件着手:1、电刀电磁干扰(EMI)的标准;2、监护仪的电磁兼容(EMC)的标准;
电刀干扰的形式包括不仅限于:空间电磁辐射,电源线、信号线、地线传导干扰,电磁耦合干扰等;
以电磁辐射为例,电刀主要的空间电磁辐射频率范围为 250khz ~ 2.5Mhz。那么应当遵循监护仪器产品使用国家、地区相关标准对于 IEC61000-4-3(空间电磁辐射抗干扰度) 等级的要求。
对于医疗仪器,标准是最为重要,这是保证仪器正常工作的核心。然后从标准着手,从设计角度,逐个解决标准兼容问题。
我的建议是1299暂时不要用来做手术室设备,因为1299本身是高度集成的芯片,这是优势,也是劣势,它使得应用场景比较狭隘,如果是分离器件设计的系统,比较容易通过调整部分器件去解决问题,1299前端除了加esd器件外,加其他运放缓冲都会影响本身功能,比如短线检测,这个是有信号反馈的,电刀我也不了解,从字面上理解,高频,能量巨大,可能不是简单的esd能吸收的,建议你咨询做过手术室监护仪的老师,除了电刀,还有那个心脏起博的高压电设备影响也很大,所以我保留1299做手术监护设备的意见,如果你们成功了,请分享下思路,技术需要共同进步