This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐DAC参考电路及DAC芯片。

Other Parts Discussed in Thread: DAC8728

如题,DAC+OP方案,需要输出电压范围(-10,+10)和(0, 5V)两种电压的脉冲发生器。刷新速率为500K和100K,数据位宽16。需要驱动后端电路。

请各位工程师指点推荐较常用的设计方案或者DAC+OP芯片组合电路,谢谢

  • DAC8728可以是双极性输出,输出范围为+-16.5V。

     如果是+-10V输出,然后再产生0~5V的话,那么可以使用运放,先给10V参考电压使之变为0~20V输入,然后再搭建比例运放。

  • Settling Time: 15μs 这个可以满足产生500K 的脉冲的条件吗?Settling Time与输出信号频率的关系可否解释一下吗?
x 出现错误。请重试或与管理员联系。