今天查询了个型号为ISO7221的芯片,双电压供电,看了下datasheet,一时没看懂 ,不知道这个芯片作何用途。是否可以作为双电平转换使用(3.3VTTL---5VTTL和5VTTL---3.3VTTL)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
meng
7221这个芯片的主要任务是隔离。就是把输入信号和输出信号隔离开。所以两侧的电源和地都不同。电平转换就大材小用了
meng
5V TTL:Vcc:5V;VOH>=2.4V;VOL<=0.5V;VIH>=2V;VIL<=0.8V。
3.3V LVTTL: Vcc:3.3V;VOH>=2.4V;VOL<=0.4V;VIH>=2V;VIL<=0.8V。
你好Seasat Liu:
我现在使用一款信号为74LVC4245的电源转换芯片,用于PXA270与模块之间的通讯,PXA270输出3.3V的TTL电平信号,模块输出5V的TTL电平信号。在使用这款芯片的时候遇到一个问题:模块与PXA270之间是两路的输入输出,一路为3.3V到5V;一路为5V到3.3V,如果选择从A到B则只能保证5V到3.3V电平转换,如果从B到A则只能保证3.3V到5V的电平转换。但是电平的传输方向由DIR引脚控制,在芯片工作的时候DIR引脚的高低电平状态固定不能改变,这样传输方向只能从A到B或者从到A。这样只能保证电平转换一路传输正确。
芯片是别人推荐的,在网上也说是经典的电平转换芯片,使用上应该没有问题,估计小弟技术欠缺没有完全理解datasheet中说的意思。
别人又推荐了一款型号为txb0108的芯片,没有方向控制引脚,不知这款芯片是否可以实现我上述的电平转换功能。