This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

自制ADS1256板子连接开发板正常,连MCU噪声大

如上面小图,单测2.5V信号时正常,目前看到的情况是在采集到的数据接近0的时候会出现这种正负38mV左右的脉冲信号,如下面大图该板接开发板正常(电源一样)。请教一下各位是否遇到类似情况。

以下是MATLAB转换的语句,主要是将2进制的补码转换为原码然后计算电压值:

for j=1:len
    if (AD_A(j)<8388608)
        AD_xA(j)=AD_A(j)/8388607*5;%   
    else
        AD_xA(j)=(AD_A(j)-16777216)/8388607*5;
    end
end

  • 你好!

    这是系统级的问题。

    请帮忙做几个测试:

    1、请用交流耦合方式测量一下电源和基准源,并上传示波器波形截图。

    2、用同样方式测量输入的2.5V信号。

    3、测量一下干扰波形的频率,是否和板子上其他元件工作频率一致,例如开关电源、时钟频率、数据信号?

  • 谢谢Billy,我后来发现在低采样频率的时候没有这个问题,最后发现是在读取数据的时候的C语言时序有问题,采样率越高问题越严重。