Other Parts Discussed in Thread: DAC5688
是否可以直接用FPGA输出3.3V给dac5688,它判断高低电平的门限是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
5688可以配置内部的IO是3.3V电平容忍还是1.8V电平容忍的
看一下寄存器26的最高位
Used to program the digital input voltage threshold levels. ‘0’=3.3V tolerate pads and ‘1’=1.8V tolerate pads.
Applies to following digital pins: CLKO_CLK1, LOCK_CLK1C, DA[15:0], DB[15:0], SYNC, RESETB, SCLK,
SDENB, SDIO and TXENABLE