2. Isolation Capacitance
Improving the isolation between the device ground and the patient ground helps to improve the system
CMR. For most portable instruments that use batteries, CMR is likely to be very high. Most typical test
methodologies to measure CMR, however, specify the minimum isolation capacitance C B at which the
system must pass the required CMR specification