使用DAC7731的过程中,总是输出不正确,输入0x8000,输出0.7V,2脚输出电压是8.7V,不是10V,两个模拟电压VCC和VSS是使用MAX232串口芯片生成的,分别是-9V和+9.4V,我想做成输出+-5V或者是正负10V的范围,不知,是否可行?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.