This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7864问题

Other Parts Discussed in Thread: ADS7864

请教专家/工程师ADS7864问题

我使用的ADS7864模数转换芯片,使用单端模拟信号输入,输入电压的范围是2.5~3v,把模拟输入信号接入CHA0+/CHA1+,CHB0+/CHB1+端,把CHA0-/CHA1-,CHB0-/CHB1-端和REFIN,REFOUT连接在一起,因为此时REFIN 和REFOUT端的电压是VREF=2.5v,不是接地。所以输出的数字量是输入电压相对于2.5v的差值的数字量还是输入绝对值的数字量?如果是输入相对于VREF=2.5V的数字量的话,如何获取模拟输入电压绝对的数字量?

谢谢!

 

  • 你好,AD转化都是以REF作为参考的,即Vmeasure=code/(2的N次方)*Vref, N 为AD的位数。

  • 你好,我还想知道的是:AD转化都是以REF作为参考的,即Vmeasure=code/(2的N次方)*Vref, N 为AD的位数。那么在ADS7864转换得到的数字量code就是对应端输入模拟量吗?还是输入模拟量减去Vref的差值所对应的数字量?比如,单端输入5V,得到的数字量code是5v的数字量还是(5v-Vref)的数字量?谢谢!