This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DDC112的一些疑问



1.  芯片的CLK和CONV引脚如果同步效果差,比如相差0.1us,会影响什么?如果影响,原理是什么?

2.  芯片CLK是用来做什么功能的?

3.  芯片可以测量电流方向从芯片流向带检测设备的信号吗?

4.  CLK速度慢一点是否有大的影响,比如1MHZ。如果有影响,会影响什么?

PS:希望可以得到诸位的指点。在此感谢!

  • 1.影响的是噪声性能,在datasheet中有描述,给出CONV建议和CLK的上升沿必须同步,误差在+-10ns范围内。
    For the best noise performance, CONV must be synchronized with the rising edge of CLK. It is recommended CONV toggle within ±10ns of the rising edge of CLK.
    2. 系统时钟。