正在设计一款产品,原本采用DAC8551,在参考电压很低的时候,输出无法达到较好的比例输出,现拟采用DAC8501,是否能实现低参考电压下依旧保持较好的比例输出?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当参考电压为0.234V时,CODE设置为15728,此时理论输出为0.0562V,实际为0.0512V,当参考电压为2.34V时CODE同样设置为15728,此时理论输出为5.62V,实际为0.555V,两次的输出比例不同,不知是什么原因,请问是否有推荐的其它产品