This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
由于功耗的考虑,AFE5816的电源,如果都使用纹波比较低的DC-DC有没有问题
我选的电源芯片纹波在20mV,算是很小的了,应该可以!
您好,
AFE5816有高频信号、模拟信号和数字信号,DC-DC有高频开关,是个开关噪声源,很容易对模拟信号和高频信号造成干扰,一般模拟信号,特别是ADC转换芯片,为使高速转换器发挥最高性能,必须为其提供干净的直流电源。高噪声电源会导致信噪比(SNR)下降 和输出中出现不良的杂散成分。一般是开关电源后加一级LDO为ADC供电。
嗯,我也知道一般是这样的,不过由于对功耗要求比较严格,用LDO的话效率太低,
能不能折中考虑,以AFE5816为例需要1.2V 1.8V 3.15V,这几个哪个对电源要求最高?
只在对电源要求高的哪个用LDO可以不?
非常感谢,能不能推荐几款LDO?