This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1256晶振选型问题

Other Parts Discussed in Thread: ADS1256, ADS1255

ADS1256对晶振要求严格吗?我看规格书里面介绍ELECTRICAL CHARACTERISTICS 采用无源晶振是从2MHz到10MHz之间,是否可以采用7.6MHz或者8MHz晶振?

  • 您好,

    可以采用7.6MHz或者8MHz晶振,相应型号可参考数据手册Table 17. Sample Crystals。晶振的精度对整个系统的性能影响很大,尽量选择精度高一点的晶振。
    晶振的选择可以参考下:www.ti.com.cn/.../sbaa104.pdf
  • 你好

         在使用ADS1255遇到一个一直解决不了的问题,采用ADS1255读取模拟量,参考电压2.5V,模拟供电5.0V,数字电压3.3V,7.6M晶振,18pf外置电容,全都配置好之后,发现晶振不起振,没有晶振的波形;或者开始一段时间晶振有输出波形也对,但工作一段时间之后,波形消失,晶振停止工作;不明白这个到底出了什么问题,

     参考2.5V使用REF3025,3.3V使用LP2985-3.3V,5V使用LP2985-5.0,

  • 我也尝试过多种不同的无源晶振,7.68M,8M都尝试过,也更换过很多匹配电容,皆不起振,请TI解答这是为啥