This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1220应用在电阻式应变片的采样精度

Other Parts Discussed in Thread: ADS1220

你好,

打扰你们了!

我们课题组计划选型于ADS1220用于电阻式应变片日本共和KFG-5-120-C1-11L1M2R的测量,采用电池低功耗供电模式,请问:在正常的情况下,ads的采样精度能到达0.01%?

  • ADS1220 是一款精密 24 位模数转换器 (ADC), 精度很高.
    采样精度能到达0.01%, 就相当于 15位 ADC 分辨率.
    不过还要考虑 Input offset voltage, Offset match, Gain error 因素
  • 您好,

    ADS1220的INL最大是±15ppm ,精度是满足您的要求的,但是ADS1220的输出精度也有供电电源的质量、输入模拟信号的噪声情况、输入模拟信号最大幅度与ADC的动态范围的匹配度、参考电压的精度、PCB的设计等也有关系。