This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我将使用DAC5681,请帮我解释一下如下问题

Other Parts Discussed in Thread: DAC5681

你好,我们将使用TI的DAC5681,做一个模拟恢复测试工作。

1-       D[15..0]P/N 如果我只使用10位的时时侯,是不是使用D[15..6]P/N更好一点

我只需要用示波器看模拟输出,没有别的应用。

2-       IOUTA1/ IOUTA2是不是一对差分形式,我看了一下是输入电流形式的,在我普通应用是,

是不是只需要外接上拉电阻即可?就要可以形成一个差分的电压信号 ?

比如说我通过100ohm上拉到3.3V,则单端输出的范围是3.1(3.3-0.2)~ 1.3(3.3-2.0)V

3-    CLKIN/CLKINC是DAC输出驱动模拟变换的时钟信号,最好与DCLKP/DCLKN完全同源同频同步

DCLKP/DCLKN是数据输入同步信号,是不是只要根据我的数据就行,比如750M都可以。