Other Parts Discussed in Thread: ADS4125, SN74AVC16244
很幸运的申请到一块ADS4125的评估板,但是经过几天熟悉评估板的用户资料和ADS4125芯片手册,我想配置成CMOS模式输出数据,经过很多次尝试,数据输出口通过逻辑分析仪查看,但是始终没有数据输出,下面我将评估板上的短接帽的连接方式写出,希望能得到大虾的指点。AD工作的时钟是通过FPGA产生的(20M),信号通过信号源产生(2M),ADS4125EVM供电3.3V,SEN短接1.8V,DFS短接BIN CMOS,RESET短接parallel,OVR短接1-2,电源短接帽均短接1-2,其他评估板默认短接方式。