This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913和914打ESD图像会抖动



我司用DS90UB913和914配对用于摄像头图像的延长,使用双绞屏蔽线,长度3-5米,线材参考的是USB线的方式,信号线双绞屏蔽,外层也是屏蔽线,屏蔽线是接地的,现在进行接触放电测试发现从2K-8K打地线图像存在抖动的问题,空气放电12KV打屏蔽线图像会抖动,整机正常不会死机和重启,就是图像会抖动,913和914是按照EVM的参考电路设计,信号线上面增加了TVS管,给相机供电的电源增加LC滤波,总电源24V入口也有TVS管,2级π型滤波器,也想了很多的办法就是不行,无非是抖动的频率和抖动的幅度的多少而已(感觉是数据有丢失,图像错位),但是始终有抖动,看能否提供一些提示,谢谢。

  • 说明信号线还是受到了干扰了。信号线双绞屏蔽,我想可能屏蔽有问题或接地还是不良。

  • 我们的线是双绞屏蔽线,屏蔽线两头分别和主机和相机的地GND相连,接头是用航空插头,外壳是直接焊在GND上面的,接地应该没有问题,现在主要问题是打线材空气放电会抖动,打GND的接触也会抖,现在问题基本集中到FPD-LINK信号线受干扰的问题上面,我看规格书上面信号线上面也没什么东西,之前还尝试过在信号线上面串联90欧的共模线圈,但是无效果。该方案看EVM是可以用在车载上面的,看能否提供一些成功案例的参考,谢谢。