This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299右腿驱动问题

Other Parts Discussed in Thread: ADS1299, ADS1298R

我使用ADS1299设计电路,发现电路的右腿驱动输出有问题,信号源输入共模信号,测量右腿驱动正常,但是接到人体上之后,右腿驱动输出就很小,我想问下是不是芯片的问题,多谢

  • 你好,能否分享下你的RLD设计原理图?

  • 电路时参照用户指南上设计的:

    REXT=1M,CXT=1nF

  • 你好,请问你的人体连接是怎样连接,有没有确认连接正常,是否做过BIAS断线检测

  • 我用的连接是一个电极接左手,一个接右手,右腿驱动不接,这时看 右腿驱动输出,只有几百毫伏,理论上人体的共模电压很大,这时候右腿驱动的输出应该是饱和的,我也用你们的ADS1298R  EVM测试过,确实是饱和。至于短线检测,我没使用芯片的功能测试,我使用万用表打的,都是导通的,这个应该没有问题,因为我接信号源输出没问题,都能放大。但是现在有一个问题就是我用信号源给定输入共模电压,右腿驱动的反馈电阻和电容也都是定值,这时候测量输出不稳定,输出两个值,两个值之间是2倍的关系,请问这又是什么问题呢?是不是芯片的右腿驱动放大器那块有问题呢?我查了很长时间,但是都不行,按说外接的只有一个电阻电容和一个保护电阻,很简单的,但是结果就是不对,所以我想问一下是不是芯片本身的问题,多谢