This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263應用諮詢

Other Parts Discussed in Thread: ADS1263

Hi,

目前选用TI的ADC采集芯片ADS1263,有些问题需要咨询一下:

       1、该芯片必须支持差分吗?

       2、第3引脚AINCOM的作用是什么,怎么使用?

       3、还有第15、16晶振引脚是不是只能接MCU的晶振,如果可以接外部晶振的话,那和使用单片机的晶振有什么区别呢?

我们的需求是:模拟采集电压值为我们的电源电压,初步确定为为5V、3.3V、1.3V这几个值,需要多通道采集,32位高精度,因为MCU资源有限,所以尽量少占用单片机的资源。

  • 您好,
    1、可以配置成单端输入。
    2、AINCOM的功能可以查看数据手册Table 5. Analog Input Pin Functions表格,功能在数据手册相应部分都有介绍。
    3、15、16脚可以使用内部振荡器也可以使用外部晶振或外部时钟,参见数据手册9.4.8 ADC Clock Modes。